Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are there replacement screws available for the 9421LF1?
Issue:
Replacement pieces are needed for the 9421LF1 Operating mechanism.

Product line:
Operating Mechanisms and Disconnect Switches

Environment:
9421LF1 9421LN1 9421LN3 9421LN4

Cause:
Repair parts

Resolution:
Yes, order the parts bag kit. Part number is 30007-500-61. This kit includes all the screws and washers needed.

The parts bag includes:
4x Mounting screws 8-32 x 3-3/4
1x On-Off Mask
1x 1/4-20 x 1 shaft bolt and nut
2x 10-32 x 3/8 self tapping screw
2x spacers
Miscellaneous additional washers