Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the Altivar ATV58 have a Profibus communication option?
Issue:
Does the Altivar ATV58 have a Profibus communication option?

Product Line:
ATV58

Environment:
All

Cause:
Profibus option

Resolution:
Yes. The Profibus communications card is part number VW3A58307U.  However, it is obsolete and there is no replacement available.