How can we help you today?

Input Circuit Breaker Selection for SURT15K and 20KRMXLI Models

"

This document is intended to add clarity to the already available information on our website regarding input circuit breaker selection for the above models

Power Input - Output Configuration

Input Circuit breaker for

SURT15KRMXLI

Input Circuit Breaker for

SURT20KRMXLI

Single Phase input

&

Single Phase output

100A / 1 pole

125A / 1 pole

Three phase input

&

Single phase output

100A / 3 pole

125A / 3 pole

Three phase input

&

Three phase output

35A / 3 pole

50A / 3 pole

Note: Convenience PDU available on the unit is attached to phase L1 and limited by the input breaker size in the event of bypass

"

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: