{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Mounting the Symmetra LX in a 2 post rack
Issue:
How do I mount a Symmetra LX in a 2 post rack?

Product Line:
Symmetra LX

Environment:
All serial ranges

Cause:
Symmetra LX ships with a 4 post rail kit only, however it is possible to safely mount the UPS system and any associated XR frames in a 2 post rack.

Resolution:
(1) SYOPT12 must be purchased and used for each Symmetra LX mainframe or extended run (XR) battery frame that is to be mounted.




Schneider Electric Saudi Arabia

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: