{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
The Matrix-UPS battery communication cable has been misplaced, what can I do?

Issue

Replacement battery communication cable for Matrix battery pack is needed.


Product Line

Matrix-UPS


Environment

All serial numbers


Cause

The cable is damaged or has been misplaced.


Resolution

The cable that provides battery communication is a standard RJ9 2 line 4 wire head set cable.  This is available at any phone accessory supplier.


Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.