How can we help you today?

Single Phase Symmetra XR Battery frame displays EF or E1


Issue

XR frame displays E1 or EF.  The mainframe indicates that an XR frame fault exists.


Product Line

Symmetra Power Array
Symmetra RM
Symmetra LX
Single Phase Symmetra XR Frames


Environment

All serial ranges


Cause

This error indicates that the XR communication card (either SYXRCC or SYAFSU16) located in the XR frame has experienced an internal problem.


Resolution

The card will need to be reseated. If reseating does not clear the fault, the card must be replaced.

For instructions on reseating the card please refer to FA157406