Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Using PowerChute Network Shutdown in a redundant UPS Scenario

Issue:
The purpose of using Power Chute Network Shutdown with a redundant UPS configuration is to confirm that an event is occurring on all UPS before sending a shutdown signal to the connected servers.

Product Line:
Power Chute Network Shutdown

Environment:
All support OS

Cause:
Informational

Solution:

Information concerning configuring PCNS with redundant UPS can be found at this linkApplication Note #98

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre