Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I view/export PowerChute Event log?

Article available in these languages: Spanish

Issue:
How can I view/export PowerChute Event log?

Product Line:
PowerChute Network Shutdown
PowerChute Serial Shutdown
PowerChute Business Edition

Environment:
All supported OS

Solution:
PowerChute Business Edition / PowerChute Serial Shutdown
To export the event log, navigate to the Event Log screen in the PowerChute user interface (UI) and click Export. This will export the event log to a text file, EventLog.txt, located in the agent directory.
The data log exists in the file <agent path>\DataLog on Windows systems and <agent path>/DataLog on Unix/Linux systems.
The default path for Windows OS is C:\Program Files\APC\PowerChute Serial Shutdown\agent



PowerChute Network Shutdown

Starting with PowerChute Network Shutdown 5.2, log in to the web UI and go to Help -> Export Support Logs

For PowerChute Network Shutdown versions 5.1 and below the event log exists in the file <install path>\group1\EventLog.txt on Windows systems and <install path>/group1/EventLog.txt on Unix/Linux systems.


The default path for Windows OS is C:\Program Files\APC\PowerChute\group1


For other logs see Schneider Electric FAQ FA241061 Files to gather when troubleshooting PowerChute Network Shutdown 3.1, 4.x, 5.x, PowerChute Business Edition 10.x, and PowerChute Serial Shutdown.