Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Upgrading a 32-bit version of PowerChute Network Shutdown to a 64-bit version on Windows
Issue:
Upgrading a 32-bit version of PowerChute Network Shutdown to a 64-bit version on Windows

Product:
PowerChute Network Shutdown

Environment:
Windows 64 bit system

Cause:
Upgrade for 32 bit OS to 54 bit

Solution:

We do not support this. We recommend that you do a full installation after manually uninstalling the old version first.

Schneider Electric Saudi Arabia