Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PowerChute Network Shutdown Configuration Files Explained

Issue:
Prior to version 3.x of PowerChute Network Shutdown (PCNS), configuration data was stored in a proprietary binary file. Users found configurations difficult to implement and distribute with this method.
From version 3.x, and above PCNS has a text-based INI configuration store for PowerChute.

Product Line:
PowerChute Network Shutdown versions 3.x, 4.x

Environment:
All supported OS

Cause:
Informational

Solution:
Please review the attached config.ini file explained.pdf


Schneider Electric Saudi Arabia

Attachment(s)
Config.ini file explained.pdf [320.46 KB]