Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the line termination module for the ATV312 CANopen network?
Issue:
Line termination module for the ATV312 CANopen network

Product Line:
ATV312 with CANopen option card

Environment:
All

Cause:
Needs a termination resistor for the CANopen network.

Resolution:
The Line Termination part number is TCSCAR013M120.