Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Schneider offer a soft start for a single phase motor?
Issue:
Soft start for a single phase motor?

Product Line:
ATS01

Environment:
All

Cause:
Needs a soft starter for a single phase motor.

Resolution:
Yes, but the offering is limited.  The ATS01N1**FT products are rated for single phase motors up to 2HP at 240V and 1/2HP at 120V.
See the attachment beginning on page 34.  Reference page 40 for part number selection.

Schneider Electric Saudi Arabia

Attachment(s)
8637CT0401R12_11.pdf [2.61 MB]