Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the cooling fan for the ATV71HD15N4?

Issue:
Is there a spare parts part number for the heatsink fan kit for the ATV61HD15N4 or ATV71HD15N4

Product Line:
Altivar 61 and Altivar 71

Environment:
AC Drives and Softstarts

Cause:
Heatsink Fan Spare or Replacement parts

Resolution:
VZ3V1205 is the heatsink fan kit.  The fan measures 3.14 by 1.5 inches.
Ordering Qty is 1 fan kit per drive.
The Kit Includes 2 Fans and the mounting adapter plate.

CTA-ID : 2061517