Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV71 how can your program the normally closed contact on the R1 relay (terminals R1B to R1C) for a run status?
Issue:
On the ATV71, trying to program the normally closed contact on the R1 relay (terminals R1C to R1B) for a run status.

Product Line:
Altivar Machines, Altivar 61, Altivar 71

Environment:
All models and serial number

Cause:
N/A

Resolution:
By default on the ATV71 drives, R2 is configured as a Drive Run contact.  To change R1 to Drive running:

Go into Main Menu > Drive Menu > 1.5 Inputs/Outputs Cfg > R1 Configuration.  Select Drive running and push Enter to save.