Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Schneider offer a drive that has connections to the DC bus for putting the regenerative voltage back onto the utility line?

Issue:
Drive offer with connections to the DC bus for putting the regenerative voltage back onto the utility line

Product Line:
Altivar Process 980

Environment:
NA

Cause:
Regenerative voltage back on the utility line

Resolution:
The Process 980 product line is an Active Front End (AFE) drive for regenerative applications.