How can we help you today?

What is the function of the " ASY " potentiometer in the RM35 relays ?

The " ASY" potentiometer is concerned with the asymmetry function between phases. You can set the percentage between 5% and 15 % of the default voltage value. If the voltage on one phase falls under the specified value, the relay will give a signal.
The difference between this function and the under voltage function is that the under voltage has a higher range. It considers the voltage as a total but it doesn't consider the asymmetry between phase waves.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre