Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What features are lost by adding the LonWorks option card VW3A21212 to the Altivar ATV212 drive?

Issue:
Some features are lost if the optional LonWorks card is added to the ATV212 drive.

Product Line:
Altivar ATV212 and ATV21

Environment:
All

Cause:
Updating to the LonWorks option card you will loose some features on the drive.

Resolution:
If the optional LonWorks card replaces the standard card, the following features are lost:

  • VIA 4 to 20mA input will be removed
  • FM analog output will be removed
  • RYA and RYC relay output will be removed.
This is also option B06 on the S-Flex enclosed package drives.