Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the power boards for the ATV21 and ATV212 series drives available?
Issue:
Availability of ATV21 and ATV212 power boards

Product line:
Altivar ATV21 and ATV212

Environment:
All models, all serial numbers

Cause:
Needs replacement power board parts

Resolution:
No, replacement boards are not available. The only replacement parts available for the ATV21 or ATV212
series drives are the heat sink fans on some of the higher HP units.
If any other part of these drives requires replacement, replace the drive.