How can we help you today?

Is the SCADA Vijeo Citect comply to the IEC standard IEC618501 ?

IEC61850 is the protocol and IEC61850-1 is classified as one of the standards  for this protocol.

We do not have IEC 61850 driver available but as a solution we can integrate device as below :-

1) Use third party gateway IEC 61850 to modbus TCPIP /Modbus serial or any other hardware gateway for which protocol is supported in Vijeo Citect.
2) Else use OPCserver.