Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum equipment & cable mounting depth for the NetShelter WX?
Issue:
Will deep IT gear fit into the NetShelter WX, and if so, how much clearance will remain for cabling?

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
The NetShelter WX is shallow which can make installation of deep rack gear challenging.

Resolution:
Please see attached file

Schneider Electric Saudi Arabia

Attachment(s)
20130918 Maximum Equipment Mounting Depth for a NetShelter WX.pdf [322.12 KB]