{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ATV312 be used to control speed of the motor with 0-10 mA?
Issue:
mA signal configuration on the ATV312 Drive

Product line:
Altivar ATV312

Environment:
All models, all serial numbers

Cause:
This drive uses terminals AI3 and COM for the mA signal.  It can be configured as 0-20mA or 4-20mA.

Resolution:
Under the I-O_ menu go to CRL3 to adjust the minimum value and CRLH to adjust the maximum value.

Schneider Electric Saudi Arabia