{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause a ILF fault on the ATV71 drive with an VW3A3501 CIC card installed?

Issue:
ILF fault on the ATV71 with an  VW3A3501 CIC card installed.

Product line:
Altivar ATV71

Environment:
All models, all serial numbers

Cause:
If the CIC card is missing the external +24vdc pwr supply the drive will trigger an ILF fault after 1 sec of being powered up.

Resolution:
Per the CIC installation manual document, atv71_controller_inside_EN_V3 page 10, it is recommended to add an external power supply part number ABL7RE2402 to the controller inside cards +24vdc and com terminals to resolve issue.

Schneider Electric Saudi Arabia