Search FAQs
What can cause an OL1 fault on the ATV21 or ATV212 drives?
Issue:
OL1 fault on ATV21/ATV212 drives.
Product line:
Altivar ATV212, ATV21
Environment:
All models, all serial numbers
Cause:
OL1 is a drive overload fault. The motor is pulling to many amps and the internal overload is tripping.
Resolution:
OL1 is an overload fault.
ITH parameter under main menu AUF is what determines the overload settings for a motor. It is normally programmed to match motor FLA.
Confirm that the motor settings including uL, F415 and F417 match your motor name plate.
Check ACC time and make sure it is not too short a ramp up time.
Set AU1 to 0.
Measure current draw by motor if possible at the output to the motor. If the current draw surpasses ITH value then it will eventually fault out on OL1 given enough time has passed.
Check for power drop in the line side of the drive.
Set PT to 0.
OL1 fault on ATV21/ATV212 drives.
Product line:
Altivar ATV212, ATV21
Environment:
All models, all serial numbers
Cause:
OL1 is a drive overload fault. The motor is pulling to many amps and the internal overload is tripping.
Resolution:
OL1 is an overload fault.
ITH parameter under main menu AUF is what determines the overload settings for a motor. It is normally programmed to match motor FLA.
Confirm that the motor settings including uL, F415 and F417 match your motor name plate.
Check ACC time and make sure it is not too short a ramp up time.
Set AU1 to 0.
Measure current draw by motor if possible at the output to the motor. If the current draw surpasses ITH value then it will eventually fault out on OL1 given enough time has passed.
Check for power drop in the line side of the drive.
Set PT to 0.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: