Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is the ATV12 output relay configured?

Article available in these languages: Spanish

Issue:
How to program the relay to a desired function.

Product line:
Altivar 12  ATV12

Environment:
All models and serial numbers

Cause:
None

Resolution:
The Altivar 12 has NO/NC programmable relay output contacts on terminals R1A-R1B-R1C.  (NO is R1A-R1C, NC is R1B-R1C).
Navigate through the menus to ConF, FULL, I-O, and then assign parameter r1 to the desired function.  See the attached file, excerpt from the User Manual, for a list of available functions.

Schneider Electric Saudi Arabia

Attachment(s)
ATV12 R1 assignment options.pdf [74.71 KB]