Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What options are there for an ATS48 Soft Start to communicate via Modbus Ethernet?
Issue:
ATS48 communication options via Modbus Ethernet.

Product Line:
Altistart  ATS48

Environment:
All

Cause:
Communications Options

Resolutions:
The softstart has built-in Modbus RTU.
Consider a Modbus to Ethernet Gateway such as the EGX150.