Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there an Ethernet TCP/IP option on the ATS22 Soft Starter?

Issue:
Does Schneider Electric offer a Modbus RTU to Modbus Ethernet TCP option on the ATS22 Soft Starter.

Product Line:
Altistart ATS22

Environment:
All

Cause:
Ethernet option on the ATS22 Soft Starter

Resolution:
The Soft Starter has a built-in Modbus port. A Modbus-to-Ethernet Gateway (EGX100SD) can be used to interface between Modbus and Ethernet communication. Gateway

Schneider Electric Saudi Arabia

Attachment(s)
Class 9998 and 9999 Control Accessories_EGX100SD Ethernet Gateway.pdf [80.39 KB]