Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can equipment be installed on the floor of a NetShelter CX or CX Mini?
Issue:
A user may want to install equipment on the floor of a NetShelter CX or CX Mini.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Equipment doesn't all fit into the U-space provided.

Resolution:
Before installing any equipment on the floor of the NetShelter CX please check with the OEM manufacturer for their installation recommendations.
The floor of the NetShelter CX and CX Mini is solid. There is no airflow being introduced from directly below the floor.