Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can you find the conduit kit dimensions for the ATV61 and ATV71 drives?
Issue:
Conduit kit dimensions for the ATV61 and ATV71 drives.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Accessories for the ATV61 and ATV71 drives.

Resolution:
You can find the dimensions in the manuals linked below:

For ATV61/71 drives 45kW (60HP) and smaller at 230V  AND less than 75kW (100HP) at 460V):
https://www.se.com/us/en/download/document/30072-451-74/

For larger HP ATV61/71 drives:
https://www.se.com/us/en/download/document/30072-451-73/