Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATS48 - runs in reverse when on a generator.

Issue:
The soft start runs the motor in reverse when in generator mode.

Product Line:
ATS48, ATS22

Environment:
All Models and serial numbers

Cause:
Motor running in reverse

Resolution:
To change the direction of the motor swap two wires feeding the soft start at the generator.