Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does the motor run forward in bypass but reverse in AFC?

Issue:
Motor runs wrong direction in AFC

Product Line:
ATV212, SFLEX

Environment:
All models

Cause:
None

Resolution:
Recommendation , swap two of the drive output leads T1-T2-T3 (motor leads). Swap the leads between the drive output terminals (load side) and drive output contactor (line side).