Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What firmware level of the Altivar 71 drive is required to run SoMove Lite?

Issue:
Unable to connect to SoMove Lite with ATV71.

Product Line:
Altivar 71

Environment:
All Models equal to and below firmware v1.5.5.0

Cause:
None

Resolution:
The compatibility table for SoMove supports the ATV71 at Firmware version level V1.5.5.0