Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the ATV12 drives plenum rated?

Issue:
Do the ATV12 have Plenum Rating?

Product Line:
Altivar ATV12

Environment:
All

Cause:
Plenum rating on the ATV12

Resolution:
No, the ATV12 drives are not plenum rated.