Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can the power dissipation specification be found for the ATV212 drives?

Issue:
Customer wants to determine if external cooling is required.

Product Line:
Altivar Machine

Environment:
Altivar

Cause:
none

Resolution:
The dissipated power is listed for each model number in the ATV212 Catalog.
See attachment for the appropriate data:

5

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Attachment(s)
ATV212 Catalog page 29.pdf [95.18 KB]