Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the conduit kit for an ATV61 or ATV71 for frame size 9?

Issue:
Part number for an ATV61HD90N4 or frame size 9 conduit kit.

Product Line:
ATV61, ATV71

Resolution:
VW3A9209 is the NEMA Type 1  Conduit Kit.  It includes a metal box with conduit knockouts.  This accessory provides a NEMA 1 enclosure rating for the drive and provides a surface area to land conduit when wall mounting the drive.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)