Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SEPAM 49RMS Application Notes

Issue
Specifics of how the ANSI 49RMS works

Product Line
Sepam 20 Series
Sepam 40 Series
Sepam 80 Series

Resolution
Thermal protection of a motor can be accomplished by using various protection elements. ANSI 49 provides over-current protection based on the magnitude of current, both past and present. The SEPAM 49RMS element uses current magnitude to model the heating effect the current has on the motor windings. The attached doc provides a detailed description of this protection function.

Schneider Electric Saudi Arabia

Attachment(s)
3000DB0811 49 RMS APP NOTE.pdf [347.16 KB]