Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the number of functions or units per type of protection for Sepam 1000+?


NOTE: Use the SFT2841, phase protection 50/51-1 tab for a better understanding of what follows.

DEFINITION: the number of functions is referred to as the number of units.


Series 20


Characteristics of 50/51 phase overcurrent protection units:

- the 50/51 function includes 2 units, identified as 50/51-1, 50/51-2

- the units are identical

- each unit can control a different output

- each unit has 2 groups of settings, called set A and set B

- this makes it possible to have 2 different groups of settings per unit

(curve, threshold, delay and other parameters)

- the setting groups may be active separately or together or according to

certain criteria (set up in SFT2841)

- only one output per unit, common to both groups of settings A and B

- each unit has its own protection setting,

- the units are dependent on the common general parameter setting "choice of

setting group A/B".



Series 40


Characteristics of 50/51 phase overcurrent protection units:

- the 50/51 protection function includes 4 units, identified as 1 to 4

- the units are identical

- each unit can control a different output

- the 4 units are grouped in 2 setting ranges, group A and group B

this makes it possible to have a total of 8 different groups of settings

(curve, threshold, delay)

- the setting groups A and B only operate as exclusive OR, i.e. 1 setting

group active at a time

- each unit has its own protection setting



Summary


For the 50/51 protection function:

- Sepam series 20 offers:

2 units with 2 groups of settings each (A and B)

i.e. a total of 4 groups of settings that can operate separately or at the

same time and that activate 2 outputs

- Sepam series 40 offers:

4 units with 2 groups of settings (A and B)

i.e. a total of 8 groups of settings that activate 4 outputs

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre