Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
490NTRJ11 Switch Initialization Cable Pinouts

Issue

This resolution provides pinout information for the 490NTRJ11 Switch Initialization Cable used for local configuration of switches. The cable connects the switch V.24 socket with a VT100 terminal or PC with appropriate terminal emulation.
re: ConneXium Ethernet Cabling System TCSESM Managed Switches Installation Manual, p/n 31007118

Product Line
Connexium

Resolution


490NTRJ11 Switch Initialization Cable

pin details


Legacy KB System (APS) Data: RESL181628 V1.0, Originally authored by WeDa on 01/16/2007, Last Edited by WeDa on 01/16/2007
Related ranges: Ethernet and TCP/IP