Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can Modbus RTU be transmitted over a modem connection?

Answer: No, since Modbus RTU is sensitive to inconsistent time delays between characters. A suggested workaround is converting the communications to Modbus ASCII for the modem part of the communications connection. See the attached document for more details.
1185.ppt

Originally article#1185

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre