Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Change the NDSCOM and the TEST parameters on a SEPAM 80 with an ACE850 module.

NDSCOM is a parameter that is not supported with the SEPAM 80 with an ACE850. The TEST parameter may be modified via the GOOSE messaging statistics found by logging into the ACE850 device. The TEST parameter will allow the GOOSE messaging system to be tested without affecting anything else. The software that we provide to help create GOOSE messaging communications within the SEPAM is the CET850 (replacement of previous SFT850). CET850 will create all of the necessary files that are associated with GOOSE messaging and will also allow these files to be easily modified by a third party software such as IECBrowser and IEDScout.