Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the ACE917?

Product Line
LPCT
ACE917

Environment
Testing

Resolution
The ACE917 is an adapter that is used to test the protection chain using as standard injection box, when the SEPAM relay is connected to LPCT APS_SENSORS.
Attached is the manual for the ACE917

Schneider Electric Saudi Arabia

Attachment(s)
LPCT type current sensors.pdf [182.81 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre