Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the level of high voltage, the isolation of XBTHPE was tested ?

Goals and Symptoms

What is the level of high voltage, the isolation of XBTHPE was tested ?

Facts and Changes

high voltage
isolation
XBTHPE
insulation

Causes and Fixes

Here are the levels that the XBTHPE terminals withstand:
Insulation resistance test :
With a voltage of 500V dc, applied between power connections and enclosure ---> Resistance < 10Mohms for new product. Resistance < 1Mohms after heat/humidity test.

Dieletric strength :
With a voltage of 500V ac , applied between each internal isolated cards and then , between all the internal card and the enclosure ---> Leackage current < 5mA.