Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What would cause "Error 182 - invalid property value ERR=00380 ERL=05400" when scrolling through my networks in ProWORX NxT?

Make sure that the checkbox for "True Type FONTS" is not checked. This can be found in the FONTS folder in the Control Panel. Look in the folder options in the Tools drop down.
image1