Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which fiber port in an NMS25102 switch is TX

Issue
The fiber optic ports in this switch are unlabeled. Which is TX and which is RX?

Product Line
ConneXium switch

Environment
499NMS25102

Resolution
The upper connection is TX the lower one RX.