Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I launch the configuration screen on my Magelis terminal?

Touching the top left and then the bottom right, one after another, will open the configuration screen if the application has the feature enabled.

The easiest way is to create a switch on the panel that accesses it directly. Simply set "operation" to system and then choose "Configuration" as the option.