How can we help you today?

How many messages can the ETG100 buffer handle before the message is lost

Issue
How many messages can the ETG100 buffer handle before the message is lost.

Product Line
ETG100

Environment
Windows 7

Resolution
Each Modbus TCP/IP connection has a separate receive buffer. The buffer size is large and
could hold many messages depending on the size of the message. Tests have shown that over
20 messages have been buffered per connection with no losses. In a worst case configuration,
the amount of time (message time-out) that the client must wait for a response to a request should
be dramatically increased

Schneider Electric Saudi Arabia