Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the value of Galvanic Insulation within TX-ports of Ethernet Connexium Switches (TCSESM family of PRODUCTS) ?

Issue
What is the value of Galvanic Insulation within TX-ports of Ethernet Connexium Switches (TCSESM)?


Product Line
Connexium TCSESM switches


Resolution
Vendor supplied specification is as follows:
Galvanic insulation is according to Ethernet standard IEEE802.3,   1500 VAC / 2250 VDC.