Quantum 984 ladder logic function block execution times
Issue
Quantum 984 ladder logic function block execution times
Product Line
All versions of ProWORX 32
Environment
Windows 7
Resolution
The following tables provide the list of execution times for the 984 ladder logic function blocks.
used in the low end (186 based cpu) and high end (486 based cpu) Quantum PLC's.
Released for: Schneider Electric Saudi Arabia