Isolation specifications for the ETG100.
Issue
Isolation specifications for the ETG100.
Product Line
TSXETG100
Environment
Windows 7
Resolution
The following are the isolation specifications for the ETG100.
- Isolation between the Ethernet POE input and +24Vdc input is 1500V.
- Isolation between the power inputs (POE and +24) and the isolated comms supply is 2500V.
- Isolation between the Ethernet input and the serial port is 1500V.
- There is only one serial port on the TSXETG100 with 2 hardware interfaces, isolation between the interfaces is 2500Vrms
Released for: Schneider Electric Saudi Arabia