Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a way to add a .EDS file to the Advantys CANopen STBNCO212 or the STBXBE2100?

Issue:
Can the Advantys canopen eds file be added other than the catalog browser?


Product Line:
Advantys Configuration Software


Resolution:
No, you only have what is available in the catalog browser in Advantys. The Advantys CANopen modules are slave devices and you can not add in .EDS files. The EDS files will need to be added to the master.