Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I know if the 140CRP93x xx or 140CRA93x xx is a RoHS compliant product ?

Issue:
Is my Quantum PLC RoHS compliant?

Product Line:
Modicon Quantum

Resolution:
The following PV's will indicate whether or not your PLC is RoHS compliant:

RoHS  140CRP93X XX       PV =>08
RoHS  140CRA93X XX       PV =>09

Non RoHS 140CRP93X XX    PV <= 07
Non RoHS 140CRA93X XX    PV <= 08